Example Custom DPD Measurement with MATLAB

A digital pre-distortion (DPD) measurement evaluates the power amplifier's (PA) performance in terms of linearity when pre-distortion is applied. This example employs user-defined DPD algorithms using MATLAB or text files.

The measurement process includes the following steps:

  1. Setting up the measurement system

  2. Configuring parameters in the N7614C software with a custom algorithm

  3. Executing the measurement and viewing results

Return to the Tutorials menu.